PN7462 flash issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 flash issue

1,865 Views
firmwareteam
Contributor I

Hello sir,

i am using PN7462 Dev kit and MCUXpresso IDE v11.4.1 , while debugging code i am getting error,

which is mention in picture, can you tell me why this error getting root cause and solution also,

firmwareteam_0-1683030557281.png

 

 

 

Best regards,

Dharm Gahlot

0 Kudos
Reply
15 Replies

1,825 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

Thanks for contacting us and interested in the NXP products.
Yes, I've checked your issue, and it is recommended that you try the following configurations.
1. MCUXpresso IDE v11.6.0 or the later.
2.SW368332\Examples\NfcrdlibEx1_DiscoveryLoop or the other example of SW368332.

To update this case, you may reply by email.
To provide confidential information or attachments, you may add that online.

Please login to our NXP technical support portal:
https://support.nxp.com/s/case/5002p00002s7JybAAE

The portal allows access to the full details of the case, including the previous communication.

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Best regards,
Kelly
Technical Support
NXP Semiconductor

0 Kudos
Reply

1,785 Views
firmwareteam
Contributor I

I try using MCUXpresso IDE v11.6.1 but still i am getting same issue.

 

i got also this error GDB stub (C:\nxp\MCUXpressoIDE_11.6.1_8255\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.6.1.202210030617\... - GDB protocol problem: Pipe has been closed by GDB. can you tell me how to solve this error.

 

 

 

 

 

0 Kudos
Reply

1,758 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

 I've recorded a video for you, please check your e-mail.

Best Regards,

kelly

0 Kudos
Reply

1,753 Views
firmwareteam
Contributor I

I try according your recorded video but still i am getting flash issue .and now i am using Mcuexpresso IDE V11.6.0 and PNEV7462B V 2.2 dev kit.

0 Kudos
Reply

1,746 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

The project building successfully and debugging failed, is this situation? If so, what type debugger did you use?

Best Regards,

kelly

 

0 Kudos
Reply

1,741 Views
firmwareteam
Contributor I

the project is building successfully and got flash error while i dump code into flash , i am using LPC Link 2 for programming ,problems occurred while i am running code in debug mode .

i am getting this error.

Flash driver "ProgramPage" timeout (500 ms) PC: 00203160 Flash driver "ProgramPage" timeout (500 ms) PC: 00203160 15: Target error from Commit Flash write: Ec: Flash driver "ProgramPage" timeout (500 ms) PC: 00203160 Debugging context: NfcrdlibEx99_DiscLoop_HIDKeyboard LinkServer DebugPN7462AU

0 Kudos
Reply

1,671 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

Your situation is very strange. So, would you like to try another board or debugger?

Best Regards,

kelly

0 Kudos
Reply

1,665 Views
firmwareteam
Contributor I

Hello @kelly

i used 4 boards and 2 debuggers but still i am getting same issue .

 

0 Kudos
Reply

1,628 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

Your situation is really special and strange. Anyway,could you try the following actions, which one can be shown or nothing?

NXF92074_0-1684988025138.png

BR

 kelly

 

0 Kudos
Reply

1,585 Views
firmwareteam
Contributor I

Hello @kelly 

I try according your last post but still getting same issue.

BR

Dharm

0 Kudos
Reply

1,567 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

Your case is very special. If the above information does not appear, it means the debugger did not find it. I have not been able to reproduce your case, so it is hard to judge what is the reason. Do you have MCU-LINK PRO? How about a different debugger and try again?

BR 

kelly

0 Kudos
Reply

1,549 Views
firmwareteam
Contributor I

i got problem while i burn my code into PN7462 Ic.i am getting debugger (LPC-LINK2 )my side also ,my problem is related to code not flash into devkit.

0 Kudos
Reply

1,537 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

Ok, I got it. So, could you share with me your file and let me try it?

BR

Kelly

0 Kudos
Reply

1,715 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @firmwareteam 

Ok, please press "shift" key and click “debug”. If the following message does not appear, go here

LPC-Link2 | NXP Semiconductors to update your driver and try again.

NXF92074_0-1684128149403.png

Best Regards,

kelly

0 Kudos
Reply

1,708 Views
firmwareteam
Contributor I

Hello Kelly 

i am still getting same error and got some time another error.


15: Target error from Commit Flash write
15: Target error from Commit Flash write
Debug port inaccessible after access at location 0x00100020
15: Target error from Read register
Wire ACK Fault in DAP access
Debugging context: NfcrdlibEx99_DiscLoop_HIDKeyboard LinkServer DebugPN7462AU (1)

or

08: Failed to set event catches
08: Failed to set event catches
Wire ACK Fault in DAP access
Debugging context: PN7462AU_ex_phExDualCcid LinkServer Release

 

if possible can we connect and resolve this issue ?

 

 

0 Kudos
Reply