PN7462 'PN7462AU_ex_phExCcid' Sample I2C not Working in "phExCcid_UsbCcid_Process"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 'PN7462AU_ex_phExCcid' Sample I2C not Working in "phExCcid_UsbCcid_Process"

Jump to solution
1,138 Views
EE_Ark
Contributor II

Hi,

I'm trying to use 'I2C MASTER HAL' with 'phhalI2CM_Transmit()' and 'phhalI2CM_Receive()' functions. I can use these functions in 'phExCcid_SystemTask' without any problem. But I can't use(can't send & receive data) them in "phExCcid_UsbCcid_Process".

 

I think the cause of the problem is about interrupt priorities. I tried to change I2C and HIF ınterrupt priorities as are initialized in "phFlasBoot.c" file.

 

/* interrupts at lowest levels */
phHal_Nvic_SetPendSVPrio(PH_HAL_INTRPT_PRIO_LOW);
phHal_Nvic_SetSysTick(PH_HAL_INTRPT_PRIO_LOW);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_BMA, PH_HAL_INTRPT_PRIO_LOW);

/* interrupts at medium prio */
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_TIMER, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_EECTRL, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_SPI, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_I2C, PH_HAL_INTRPT_PRIO_MED);

phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_Common_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_01_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_02_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_03_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_04_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_05_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_06_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_07_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_08_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_09_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_10_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_11_Isr, PH_HAL_INTRPT_PRIO_MED);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_GPIO_12_Isr, PH_HAL_INTRPT_PRIO_MED);

/* interrupts at high prio */
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_CLIF, PH_HAL_INTRPT_PRIO_HIGH);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_HIF, PH_HAL_INTRPT_PRIO_HIGH);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_CTIF, PH_HAL_INTRPT_PRIO_HIGH);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_PMU, PH_HAL_INTRPT_PRIO_HIGH);
phHal_Nvic_SetInterruptPrio(PHHAL_NVIC_PCR, PH_HAL_INTRPT_PRIO_HIGH);

/* interrupts at real time prio */
phHal_Nvic_SetSvCPrio(PH_HAL_INTRPT_PRIO_REALTIME);

 

It didn't solve anything. What can I try to fix the problem?

0 Kudos
Reply
1 Solution
1,066 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @EE_Ark 

Please refer to the application architecture of the phExCcid example.

PN7462AU CCID reader application has 4 modules:  USB ISR, system task, CL task, CT task.

danielchen_0-1641475244680.png

phhalI2CM_Transmit()' and 'phhalI2CM_Receive() are blocking calls, they wait for the i2c transaction to complete.  They can work in task context.  as you mentioned, they can work in 'phExCcid_SystemTask' without any problem.  But not good to work in an ISR.  we can not call a blocking call in an ISR.

 USB ISR is responsible for sending and receiving the CCID class commands through the bulk out, bulk in and interrupt endpoints.

I would suggest you perform the I2C transmit/receive operations in a task. or you can trigger an event in USB ISR, and wait the event in a task, then perform i2c sending/receiving in this task

 

Regards

Daniel

 

View solution in original post

0 Kudos
Reply
2 Replies
1,133 Views
EE_Ark
Contributor II

IF I use 'SET_HIF_USB_LOW_PRIORITY' it looks like it can communicate a few bytes but after that I receive a hard page fault.

0 Kudos
Reply
1,067 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @EE_Ark 

Please refer to the application architecture of the phExCcid example.

PN7462AU CCID reader application has 4 modules:  USB ISR, system task, CL task, CT task.

danielchen_0-1641475244680.png

phhalI2CM_Transmit()' and 'phhalI2CM_Receive() are blocking calls, they wait for the i2c transaction to complete.  They can work in task context.  as you mentioned, they can work in 'phExCcid_SystemTask' without any problem.  But not good to work in an ISR.  we can not call a blocking call in an ISR.

 USB ISR is responsible for sending and receiving the CCID class commands through the bulk out, bulk in and interrupt endpoints.

I would suggest you perform the I2C transmit/receive operations in a task. or you can trigger an event in USB ISR, and wait the event in a task, then perform i2c sending/receiving in this task

 

Regards

Daniel

 

0 Kudos
Reply