PCF85063A sometimes reporting time 00/0/0:0/0/0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF85063A sometimes reporting time 00/0/0:0/0/0

555 Views
ombokdouglas
Contributor I

Hi

I have worked on a board that has PCF85063A together with microchip MCU (PIC24FJ128GL306). We have over 10,000 units in the field that constantly log data. The RTC works well however there are times when the chip time resets to 00. The date reported is 00/00/00:00/00/00(YY/MM/DD:HH/MM:SS).Sometimes, this happens temporarily then it resumes to the correct date and time while sometimes the it does not resume to the correct time. While this happens the time still increments well(seconds and minutes). What could be the issue here. This is the circuit

ombokdouglas_0-1692877538297.png

 

What could be the issue here?

0 Kudos
Reply
1 Reply

529 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello ombokdouglas,

I hope all is great with you. Thank you for using the NXP communities.

I would like to add some recommendations about the power up timing that you may consider:

We require the VDD to go up very quickly (< 8ms), or else there is a chance of corrupted registers due to POR failure.

Would it be possible for you to ensure that such a condition is met?

I hope this information helps.

Regards,

David

0 Kudos
Reply