PCAL6416A input current when Vi=0V and VDD(P)=0V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCAL6416A input current when Vi=0V and VDD(P)=0V

520 Views
sylvainbouriot
Contributor I

I want to use PCAL6416A on a new projet.
In the datasheet, the  input current (HIGH-level input current and LOW-level input current) is specified for  VI = VDD(P)and  VDD(P) = 1.65 V to 5.5 VVDD(P) = 1.65 V to 5.5 V.
Is it allowed to apply  a 3.3V or 5V voltage on an input pin when the the PCAL6416 is not powered (Vi=0V and VDD(P)=0V)?
If yes, what is input current ?

Best Regards.

Sylvain

0 Kudos
Reply
0 Replies