PCAL6408A voltage design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCAL6408A voltage design

622 Views
morgan_jiang
Contributor I

As mentioned in the PCAL6408A  datasheet:

There are two supply voltages for PCAL6408A: VDD(I2C-bus) and VDD(P).

VDD(I2C-bus) provides the supply voltage for the interface at the master side (for example, a microcontroller) and the VDD(P) provides the supply for core circuits and Port P.

The bidirectional voltage level translation in the PCAL6408A is provided through VDD(I2C-bus).

VDD(I2C-bus) should be connected to the VDD of the external SCL/SDA lines.

This indicates the VDD level of the I2C-bus to the PCAL6408A, while the voltage level on Port P of the PCAL6408A is determined by the VDD(P).

In Our design, VDD(I2C-bus) and the high-level voltage of Port P are equal (both 3.3V), can VDD(I2C-bus) and VDD(P)  can be connected together?

Tags (1)
0 Kudos
Reply
1 Reply

552 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

There is no problem to connect both supply voltages together, the PCAL6408A will work correctly.

Best regards,

Tomas

0 Kudos
Reply