PCA9745B SDO high-impedance state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9745B SDO high-impedance state

1,463件の閲覧回数
daniel_flueckig
Contributor I

Hi, I use the PCA9745B on a shared SPI bus system with other three non PCA9745B devices in parallel.

Problem: The SDO output signal goes not in the high-impedance state when /CS is high like described in the datasheet section 8.1 :

"8.1 SPI-compatible 4-wire serial interface signals
CS — The active LOW chip select line is used to activate and access the SPI slaves. As
long as CS is HIGH, all slaves will not accept the clock signal or data, and the output SDO
is in high-impedance state. Whenever this pin is in a logic LOW state, data can be
transferred between the master and all slaves."

Regards Daniel

0 件の賞賛
返信
5 返答(返信)

1,266件の閲覧回数
ebeppler03
Contributor I

We are also encountering this issue - We have had no luck in debugging - Has anyone else found a resolution?

0 件の賞賛
返信

1,249件の閲覧回数
aschauss
Contributor I

The SDO pin did not appear to go into a high impedance state when the chip was not selected. The solution that we went with was to add a tristate buffer before the SDO pin.

1,358件の閲覧回数
Schauss
Contributor I

Daniel, were you able to resolve your issue with the PCA9745B SDO pin not going to high impedance when /CS was high.  We are struggling with the same issue.

0 件の賞賛
返信

1,362件の閲覧回数
aschauss
Contributor I

Daniel, did you resolve the issue with the SDO not going to its high impedance state, when /CS is high? We seem to be having the same issue.

0 件の賞賛
返信

1,403件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Daniel,

Sorry for the delayed response. 

I tested the /CS and SDO pins on PCA9745B demo board today. MCU GPIO pin can drive SDO pin to either high or low level while /CS pin is high (PCA9745B is de-activated), so I could not duplicate what you are seeing.

Could you post here part of your schematic to double check it?

Best regards,

Tomas

0 件の賞賛
返信