PCA9698使用前咨询

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9698使用前咨询

655件の閲覧回数
150973860
Contributor I

我有个产品想用PCA9698DGG这个芯片扩展IO,只做输出使用,我想请问:

1、由于我MCU引脚有限,只有三根引脚用于扩展,我想接SDA、SCL和RESET,因为只做输出使用,请问OE输出使能引脚可以直接接低电平吗?

2、因为只做输出使用,INT引脚可以不接吗?

3、我扩展IO的目的是模拟多路SPI接口,请问这个芯片的响应速度是否可以满足?(我使用的SPI速度不是很高)

 

非常感谢!

0 件の賞賛
返信
1 返信

556件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

For your questions please see comment:

1:Please read datasheet describe about OE function:

-----

• When a LOW level is applied to the OE pin, with OEPOL = 0 (register 2Ah, bit 4) or a
HIGH level is applied to the OE pin, with OEPOL = 1 (register 2Ah, bit 0), all the I/Os
configured as outputs are enabled and the logic value programmed in their respective
OP registers is applied to the pins.
• When a HIGH level is applied to the OE pin, with OEPOL = 0 (register 2Ah, bit 0) or a
LOW level is applied to the OE pin, with OEPOL = 1 (register 2Ah, bit 0), all the I/Os
configured as outputs are 3-stated.

-----

2:Yes

3:what's your SPI speed?

Thanks!

0 件の賞賛
返信