Hello,
I would like to use the PCA9685 with 3.3v mcu (vcc and also i2c pins =3.3v) and to output a pwm signal that ranges from 0v to 5v (0%-100%) instead of 0-3.3v range.
Can you please advice:
1. If it can be done by supplying 5v to the outputs servos and leds with the pwm output?
2. Does it have an internal level shifter or other solution? if not, if adding a 1 channel level sihfter between the 3.3v mcu and the pca9685 scl/sda will solve this issue?
Thank you in Advance!
已解决! 转到解答。
Hello Barg,
Yes, the PCA9306 is sufficient for SDA and SCL lines. The OE pin can be connected directly to GND unless you want to use it for hardware LED blinking by toggling it.
Best regards,
Tomas