PCA9615 - voltage level translator for 1,2V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9615 - voltage level translator for 1,2V

487件の閲覧回数
matthiasneth
Contributor I

Which voltage level translator can be used in combination with the PCA9615 to connect an I2C device that needs 1,2V as high signal level level and maximum 0.36V as low level  ?

The device will have to recognize the 0.5V low level output of the PCA9615 as low level input.

any recommendations ?

Thank you and Best Regards

0 件の賞賛
0 返答(返信)