PCA8575 Residual Voltage on IO After VCC loss of Power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA8575 Residual Voltage on IO After VCC loss of Power

335 Views
danielhorii
Contributor I

Hello, we currently have a scenario where our PCA8575 IO expander when it loses 3.3V power (due to the normal power off process), will have two IO pins, specifically pin 13 and pin 20 will be exposed to a separate 3.3V on the order of 100 ms. Is this permissible? Could we expect future damage or degradation in the future?

Thanks all.

0 Kudos
2 Replies

296 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do  pin 13 and pin 20  have decouple capacitors?

0 Kudos

259 Views
danielhorii
Contributor I

No they do not.

0 Kudos