On the amplitude of 32.768KHz crystal oscillator of PCA21125

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

On the amplitude of 32.768KHz crystal oscillator of PCA21125

772 Views
wanqiangsheng
Contributor I

Hello, I have an amplitude problem about crystal 32.768khz of PCA21125:
The oscilloscope shows that the frequency of the crystal signal is 32.76khz.
The peak to peak value of the waveform OSCI is 0.8V, the positive peak reaches 0.5V, and the negative peak reaches -0.3V.
The peak to peak value of the waveform OSCO is 0.4V, the positive peak reaches 0.4V, and the negative peak reaches 0V.
I want to know, is the amplitude of such a wave in the normal range? Can the amplitude of such a crystal signal ensure that PCA21125 works normally?

0 Kudos
1 Reply

672 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please download UM10301 page7 table2 shows the detail information of CLOCK spec.

Thanks!

0 Kudos