Hi.
I am developing a product with Nxp NTAG: https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf For some reasons I need to power off component via software (it is attached to i2c bus).
Is possibile power off module via software in order to avoid to modify schematic breaking Vcc wire?
Thanks and regards.
Fabrizio.
Hi @fcrudo,
The NT3H2111 t has its own form of soft reset as described in Datasheet, page 39, chapter "9.3 I²C soft reset and NFC silence feature", which is a soft reset of the I2C subsystem, and NFC disable, in which the NFC demodulator is disabled.
if NFCS_I2C_RST_ON_OFF is set, the I2C soft reset feature interprets an I2C repeated start (no I2C stop in between) as a command to execute a soft reset of the I2C subsystem.
Do you need to power off the NTAG for energy consumption?
Best regards,
Julián.
Hi Julián.
Thanks a lot for response.
Reading manual seems that NFCS_I2C_RST_ON_OFF is perfect for my target.
I will try to change and test if NFC demodulator will be disabled.
Do you need to power off the NTAG for energy consumption?
No, I need to disable nfc for specific period and enable when some development will be ready.
Regards.
Fabrizio