When using PCA9614, is it OK to apply power to VDD(A) but not VDD(B)? I couldn't find power sequencing requirements in the datasheet.
The specific situation I'm wondering about is:
If VDD(A) is +5V and EN is asserted (also to +5V), can VDD(B) be left unpowered?
- In this situation are the SDA & SCL pins Hi-Z? (ie can other i2c devices connected to these pins continue to function?)
- In this situation will the VDD(B) pin ever source current and parasitically power other parts of the circuit?
- Is any of this different if the EN pin is driven low instead?
Thank you.