NVT2008BQ LEVEL TRANSLATOR OPERATION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVT2008BQ LEVEL TRANSLATOR OPERATION

574 Views
bijumohankc
Contributor II

We are using the level translator IC -NVT2008BQ in our design.But in our application , same voltage will be used at the both sides of the level translator in certain times (VADJ_1V8,it can be 1.2V or 1.8V). In datasheet its mentioned like "The applied voltages at Vref(A) and Vpu(D) should be such that Vref(B) is at least 1 V higher than Vref(A) for best translator operation." Could you please confirm whether this level translator can work with same voltages on both sides(Its not clear from the datasheet page.9) ? Or any other modification required for the following design which is attached with this?

0 Kudos
1 Reply

498 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

This question is being solved internally (Case #00166169). 

0 Kudos