NTSX2102 2.8v

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTSX2102 2.8v

631 Views
amarasaif
Contributor II

Hello I use the S32K148 micro controller supplied with 3.3V which comunique with a Can tranceiver supplied with 5V
the voltage at the terminal of A1 and A2 is 2.8V
B1 and B2 output a voltage which oscillates between 2.8V and 5V.
is it normal to behave like this?
I share with you my schematic as an attachment
thank you for your support

0 Kudos
4 Replies

597 Views
guoweisun
NXP TechSupport
NXP TechSupport

0.1uF should be OK,pull up resistors should be 2.2K.

 

0 Kudos

599 Views
guoweisun
NXP TechSupport
NXP TechSupport

0.1uF should be no problem.

Pull up resistor should be added in A/B side,such as 2.2K.

0 Kudos

622 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you have decouple capacitors of VCCA/B side?

do you have pull up on A/B side?

0 Kudos

616 Views
amarasaif
Contributor II

Hi Sir

Thank for your answer.

I have 100nf 16V  capacitor for VCCA and VCCB

i dont have a pull up in A/B

shoud place a capacitor and if the valu of capacitor is OK?

what is the valu of A/B pull up resistor ?

thank you

0 Kudos