NTB0102 unused pin termination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTB0102 unused pin termination

Jump to solution
925 Views
andy_kim
Contributor IV

Hello,

I'd like to apply NTB0102 voltage level translator instead of 74AVC2T45 for SPDIF signal line.

Let me attache the picture of the circuit for your refer.

 

As you might know, NTB0102 is 2-bit voltage level translator.

How should I do termination for the 1-bit pin which is not used? Floating or Connecting to GND?

0 Kudos
1 Solution
922 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Andy,

The A and B sides of an unused I/O pair must be held in the same state, both at VCCI or both at GND. I would recommend to connect the unused I/O pair to GND.

JozefKozon_0-1622106050403.png

With Best Regards,

Jozef

View solution in original post

0 Kudos
2 Replies
923 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Andy,

The A and B sides of an unused I/O pair must be held in the same state, both at VCCI or both at GND. I would recommend to connect the unused I/O pair to GND.

JozefKozon_0-1622106050403.png

With Best Regards,

Jozef

0 Kudos
918 Views
andy_kim
Contributor IV

Dear Jozef

Thank you for your prompt reply.

Andy