NHS3152 I2D Offseet Current settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NHS3152 I2D Offseet Current settings

704 Views
bmeyer
Contributor II

Hello NXP:

When setting up the I2D converter, there are two I offset settings but no description as to magnitude or sign. Plus no explanation of how these are used.

0 Kudos
3 Replies

628 Views
driesmoors
NXP Employee
NXP Employee

Hello @bmeyer

Did you have a look at the firmware documentation?

Check <SDK>/docs/firmware.html > Documentation of the low-level HW block drivers > i2d: Current to Digital converter driver

 

Kind regards,
Dries

0 Kudos

690 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @bmeyer ,

 

Unfortunately there is no detailed documentation available for the I2D block. but if you are willing to share the expected current range and an electrical model of the current source, we can assist you setting up the system.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

670 Views
bmeyer
Contributor II

Hello Kan:

Thanks for the reply. I'm not sure what I could share. I'm trying to figure out how the I2D system works on the NHS3152 IC. Although, settings without sufficient explanation make understanding difficult. 

0 Kudos