Migrating from MPC5643L to MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Migrating from MPC5643L to MPC5744P

776 Views
pabloprieto
Contributor I

Hi guys,

I am trying to migrate a hardware from MPC5643L to MPC5744P following the document attached in the following link:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4624.pdf

According to the document, the chips are pin2pin compatible except 3 pins that if you have connected to Vdd it couldnt be a problem.

I have created a small design with a blinking led, and i am able to erase and program the microprocessor but when i try to run the program it gets stucks and the led never blinks.

I am generating the .elf with the MPC5744P  MCTOOL BOX and the same program generated with th MPC5643L MCTOOL BOX for the MPC5643L is working without any problem.

Has anyone experienced this type of problem? Any idea PLEASEEEEE.

Thanks a lot in advance.

Pablo

Tags (3)
0 Kudos
3 Replies

441 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I do not have an experience with the RAppID tools, so I guess you should use their support directly on the rappid@freescale.com, if you think there is issue with the MCTOOLBOX.

However attached you may find simple example for PLL init tested on the MPC5744PEVB. It also sets PB6(B9) pin as output for clock measurement. You may test it on your board to see the MCU is running.

Regards,

Petr

441 Views
pabloprieto
Contributor I

Thanks PetrS,

Witch IDE do you use to compile the project?

Regards,

Pablo

0 Kudos

441 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Pablo,

it is done in GreenHills IDE v. 6.1.4

Regards,

Petr

0 Kudos