Marvell 88MW300 QFN-68: Confirmation as non-adaptive equipment under EN 300 328 V2.2.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Marvell 88MW300 QFN-68: Confirmation as non-adaptive equipment under EN 300 328 V2.2.2

跳至解决方案
1,150 次查看
ms48154
Contributor II

In order to clarify our status for regulatory compliance, I would like to receive confirmation that the product derived from Marvell 88MW300 QFN-68 is a non-adaptive equipment under EN 300 328 V2.2.2.  To be more specific, related product is Azurewave AW-CU300 IEEE 802.11 b/g/n WLAN Microcontroller Module:

 

EN 300 328 V2.2.2 info

  • Adaptive equipment is capable of using an automatic mechanism which allows the equipment to adapt to its radio environment by identifying other transmissions on the operating frequency.
  • Non-adaptive equipment does not use such an automatic mechanism and hence is subject to certain restrictions with respect to using the medium (see clause 4.3.1.6 and clause 4.3.2.5 for Medium Utilization factor) in order to ensure sharing with other equipment.

Thank you in advance.

 

0 项奖励
回复
1 解答
1,134 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

here is the document , you can download it from nxp website.

https://www.nxp.com.cn/docs/en/application-note/AN12910.pdf

 

Have a good day!

Regards,

weidong

在原帖中查看解决方案

4 回复数
1,135 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

here is the document , you can download it from nxp website.

https://www.nxp.com.cn/docs/en/application-note/AN12910.pdf

 

Have a good day!

Regards,

weidong

1,142 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

See below, plese!

weidong_sun_0-1627372401594.png

So it is an adaptive device.

 

Have a good day!

Regards,

weidong

0 项奖励
回复
770 次查看
ms48154
Contributor II

To whom it may concern:

For your information, we are currently manufacturing Wi-Fi Adapter with Azurewave AW-CU300 Wi-Fi module based on Marvell 88MW300.

We are now planning to carry out RED certification testing in Europe and would like to check availability of a SW tool to manually set the Wi-Fi channel, bandwidth, bit rate, etc. as part of this RED testing for Wi-Fi Adapter.

Your feedback is appreciated.  Thank you.

0 项奖励
回复
1,136 次查看
ms48154
Contributor II

Hello Weidong:

 

Thank you for your reply.

If possible, could you please help be more specific about your reasoning?  Based on which specific information from the Marvell product datasheet were you able to make this judgment that it is adaptive instead of non-adaptive?  Thank you in advance.

标记 (1)
0 项奖励
回复