MXRT1020 Flex SPI with SPT tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MXRT1020 Flex SPI with SPT tool

238 Views
Shealtiel
Contributor I

Hello,

I'm facing issues in executing flex spi nor polling transfer example using SPT tool (authenticated HAB) I'm using.

But debugging it works fine.

Please check this issue.

I'm using

(MXRT1020 , SDK_2_15_000_EVK-MIMXRT1020 , MCUXpresso IDE v11.9.1_2170, MCUXpresso Secure Provisioning v8)

Shealtiel Elizer

 

0 Kudos
Reply
3 Replies

210 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Could you provide more specific details on the issue you are having?

Best regards,
Omar

0 Kudos
Reply

197 Views
Shealtiel
Contributor I

Wanted to flash FLEX SPI example code using authenticated HAB (SPT TOOL), it was written successfully but my code was not running after I switched it into boot mood.

0 Kudos
Reply

187 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to AN12681, there you can find detailed steps to use HAB. It may be possible that HAB is not well implemented so the image is not executed when flashing. 

Best regards,
Omar

0 Kudos
Reply