MRFE6VP61K25HR5/H6 RF Power LDMOS Transistors MODULE Difference.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MRFE6VP61K25HR5/H6 RF Power LDMOS Transistors MODULE Difference.

183 次查看
ISLEE
Contributor I

 MRFE6VP61K25HR5/H6

The difference between the two parts is not clearly stated in the data sheet.

 H5 / H6 - Please check if there is a difference between the two parts.
Thank you.

  

ISLEE_0-1716944158567.png

 

 

0 项奖励
回复
1 回复

161 次查看
Beckywang
NXP TechSupport
NXP TechSupport

Hello Islee

The difference is packing only. It is the same MRFE6VP61K25H device. https://www.nxp.com/part/MRFE6VP61K25H#/

R5 means

  • Packing: REEL-Reel 13" Q2/T3 in SmallPack
  • Min. Package Quantity: 50

R6 means

  • Packing: REEL-Reel 13" Q2/T3
  • Min. Package Quantity: 150

 

 

0 项奖励
回复