MPC8313eRDB REVA4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8313eRDB REVA4

1,446 Views
admin
Specialist II
Dear all,
Now I use  MPC8313eRDB REVA4 board.I tried to use MPC8313E_RDB_K26_20080613 BSP on my board.The problem took place that the Marvell's PHY could not work.I would like to known if the MPC8313E_RDB_K26_20080613 BSP can beed used on MPC8313eRDB REVA4 board?if not,I would like to know why?
Thanks.
0 Kudos
Reply
3 Replies

646 Views
admin
Specialist II
You need the REVB RDB board to use that BSP.

-joe
0 Kudos
Reply

645 Views
Veiga
Contributor I
Hi,

I think i have the same problem. Marvell's PHY can't work on linux (uboot is ok). I am trying to use MPC8313E_RDB_K26_20081226 on my MPC8313eRDB REVA3 board... and I thought it was back-compatible. Is it not?

Where can i found a BSP compatible with my board revision?

 
Thanks for any help.

-veiga

0 Kudos
Reply

646 Views
Veiga
Contributor I

 Hi,

 

It works with MPC8313E_RDB_K26_20070831.

I think MPC8313E_RDB_K26_20081226 is not compatible with REVA boards!

 

-veiga

 

0 Kudos
Reply