Recently, I implemented a CAS(compare and swap) based on PowerPC instruction lwarx and stwcx as an inline assembly function.
1 In e200z6 PowerPCTM Core Reference Manual pp124
Reservation granularity is implementation dependent. The e200z6 does not define a reservation granule explicitly; it is defined by external logic. When no external logic is provided, the e200z6 does not compare addresses; thus, the effective implementation granularity is null.
2 In PowerPC Microprocessor Family: The Programming Environments Manual for 64-bit Microprocessors pp423
When the RESERVE bit is set, the processor enables hardware snooping for the block of memory addressed
by the RESERVE address.
/******************************************************************/
If the processor detects that another processor writes to the block of memory it
has reserved, it clears the RESERVE bit.
/******************************************************************/
3 However, I found this in MPC5668x Microcontroller Reference Manual pp364
/******************************************************************/
Reservation management logic external to the e200z6 is not implemented.
/******************************************************************/
Who can help me, please?
解決済! 解決策の投稿を見る。
> Who can help me, please?
You have already proved the hardware can't do what you want, and written a very good post on that subject with good references.
So what help do you want? I'm assuming you want help on implementing semaphores or mutexes, or a mechanism to support same.
There are lots of books on that subject. Not all CPUs support CAS type instructions, so people have been inventing other ways to do this for a long time. I'd suggest you start here:
http://en.wikipedia.org/wiki/Mutex#Software_solutions
You should be looking for sample code that implements semaphores/locks on existing CPU architectures without reservation. There may be linux ports for various platforms that do all of this already.
Tom
> Who can help me, please?
You have already proved the hardware can't do what you want, and written a very good post on that subject with good references.
So what help do you want? I'm assuming you want help on implementing semaphores or mutexes, or a mechanism to support same.
There are lots of books on that subject. Not all CPUs support CAS type instructions, so people have been inventing other ways to do this for a long time. I'd suggest you start here:
http://en.wikipedia.org/wiki/Mutex#Software_solutions
You should be looking for sample code that implements semaphores/locks on existing CPU architectures without reservation. There may be linux ports for various platforms that do all of this already.
Tom
Actually, I just want to make sure what I stated is right. Because I don't find an explict declaration from freescale that MPC5668G doesn't support inter-core CAS.Maybe I did not express myself clearly.
Thanks!
The MPC5668 is an assymetric part.
The E200Z6 core has FPU, MMU and a cache. The E200Z0 core doesn't have any of these. The second core isdocumented as "Additional e200z0 core to pre-process incoming communication data from high-speed networks".
This can't easily run SMP. The second core is meant as a dedicated IO Processor running its own separate code. You're probably meant to implement memory-based message passing that doesn't require hardware-based semaphores.
Tom