MPC555 QSPI register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC555 QSPI register

2,288 Views
csjessid
Contributor I
Hi,
I´m trying to set up a QSPI communication with the MPC555 (master) and a Fujitsu Microcontroller (slave). I wrote an external c-function in which I set the registers (global reg, control reg, ...). In Simulink I created a method to read these registers an send it via CAN (just to control, if its set correctly). But every time I set just a single bit in the control register 2 or 3 I don´t receive an answer from the called functions. As if the communication was disabled or something... I already took care of the fact to write the registers in the specified order, but I can´t find a solution. Does anybody know, how to initialize the QSPI or is it supposed to be that way???
 
kind regards
 
Christian
0 Kudos
Reply
1 Reply

887 Views
leblanc
Contributor I
Anyone with any tips on good practices when debugging spi communication.  Could be a problem with my initialization or with my external eeprom device.  i have an oscilloscope but don't know how to use it as a protocol analyzer.  [hyperterminal?, cheap external equipment???]  want to know what others use.


First is my intialization which includes sci0 and spi.
Then i include my 2 functions which set commands and transfers data out the queue.  Do i have the right concept?  [more curious on how to use received buffer ram(read function).]


void setup_qsmcm()
{
    //Has 2 sci interfaces and has 1 qspi

    QSMCM.QSMCR.B.STOP = 0;
    QSMCM.QSMCR.B.FRZ1 = 0;
    QSMCM.QSMCR.B.SUPV = 0;
        //keep registers access as global not restricted


    //Setup Interrupt Pins
    QSMCM.QDSCI_IL.B.ILDSCI = 5;                 // define SCIIRQ at level 5
    QSMCM.SCC1R1.B.TIE = 0;                        // disable transmit interrupt;
    QSMCM.SCC1R1.B.TCIE = 0;                    // disable transmit complete interrupt;
    QSMCM.SCC1R1.B.RIE = 1;                        // enable receiver interrupt;
    QSMCM.SCC1R1.B.ILIE = 0;                    // disable idle-line interrupt;


   
    //Before changing register values, allow the SCI to complete the current transfer,
    //then disable the receiver and transmitter.


    QSMCM.SCC1R0.B.SC1BR = 40000000/32/9600;     // Set 9600 Baud 40000000/32/9600; = 0b0000010000010;
   
    //SCI Control Register
    QSMCM.SCC1R1.B.LOOPS = 0;
    QSMCM.SCC1R1.B.WOMS = 0;                    // normal CMOS output [only when configured as output txd]
    QSMCM.SCC1R1.B.ILT = 0;                     // idle-line; 0=short; 1=long
    QSMCM.SCC1R1.B.PT = 0;                        // 0 = even; 1 = odd
    QSMCM.SCC1R1.B.PE = 0;                        // parity disabled
    QSMCM.SCC1R1.B.M = 0;                        // mode select: 0 = 10 bit mode; 1 = 11 bit mode
    QSMCM.SCC1R1.B.WAKE = 0;                    // wakup by address mark; 0 = idle line detection; 1 = address mark (last bit set)
    QSMCM.SCC1R1.B.RWU = 0;                        // normal receiver operation (received data recognized); 1 = wakeup mode enabled (ignore data until awakened)
    QSMCM.SCC1R1.B.SBK = 0;                        // send break 0=normal; 1 = break frame(s)   

    QSMCM.SC1DR.R = 0x00;                        // intialize first char to transmit, aka, null

   
    QSMCM.SCC2R0.B.SC2BR = 0;                    // disable baud rate generator for sci2
    QSMCM.SCC2R1.B.LOOPS = 0;
    QSMCM.SCC2R1.B.WOMS = 0;
    QSMCM.SCC2R1.B.ILT = 0;
    QSMCM.SCC2R1.B.PT = 0;
    QSMCM.SCC2R1.B.PE = 0;
    QSMCM.SCC2R1.B.M = 0;
    QSMCM.SCC2R1.B.WAKE = 0;
    QSMCM.SCC2R1.B.TIE = 0;
    QSMCM.SCC2R1.B.TCIE = 0;
    QSMCM.SCC2R1.B.RIE = 0;
    QSMCM.SCC2R1.B.ILIE = 0;
    QSMCM.SCC2R1.B.RWU = 0;
    QSMCM.SCC2R1.B.SBK = 0;
    QSMCM.SCC2R1.B.TE = 0;
    QSMCM.SCC2R1.B.RE = 0;


    //desktop to controller communication
    QSMCM.SCC1R1.B.TE = 1;                         // Enable Transmitter
    QSMCM.SCC1R1.B.RE = 1;                         // Enable Reciever
   
   
    /*
        // when sci as a queue
        QSMCM.SCRQ[0].B
            // 16 bits; 16 blocks
        QSMCM.SCTQ[0].B
            // 16 bits; 16 blocks
    */
   
   
    // above 2 sci initialized
    //-----------------------------------------------------------------------
    // below 1 qspi initialized
       
    QSMCM.SPCR1.B.SPE = 0;        //disable qspi


    // PORTQS Pin Assignment Register (Basically prepare to be setup as a QSPI)
    QSMCM.PQSPAR.B.QPAPCS3 = 1;                 // 1 = Pin is assigned PCS3 function else GPIO pin
    QSMCM.PQSPAR.B.QPAPCS2 = 1;                    // 1 = Pin is assigned PCS2 function else GPIO pin
    QSMCM.PQSPAR.B.QPAPCS1 = 1;                 // 1 = Pin is assigned PCS1 function else GPIO pin
    QSMCM.PQSPAR.B.QPAPCS0 = 1;                 // 1 = Pin is assigned PCS[0] function else GPIO pin
    QSMCM.PQSPAR.B.QPAMOSI = 1;                 // 1 = Pin is assigned MOSI function
    QSMCM.PQSPAR.B.QPAMISO = 1;                 // 1 = Pin is assigned MISO function


    //PORTQS Data Direction Register (DDRQS)
    QSMCM.DDRQS.B.QDDPCS3 = 1;
    QSMCM.DDRQS.B.QDDPCS2 = 1;
    QSMCM.DDRQS.B.QDDPCS1 = 1;
    QSMCM.DDRQS.B.QDDPCS0 = 1;
        // pins serve as chip selecter; therefore enable all PCS pins as outputs.
        // currently only using QDDPCS0

    QSMCM.DDRQS.B.QDDSCK  = 1;                     // 1 = Pin direction is output
    QSMCM.DDRQS.B.QDDMOSI = 1;                     // 1 = Pin direction is output; master output slave input
    QSMCM.DDRQS.B.QDDMISO = 0;                     // 0 = Pin direction is input; master input slave ouput

   
    QSMCM.SPCR0.B.MSTR = 1;                        // 1 = QSPI is the system master and can initiate transmission to external SPI devices.
    QSMCM.SPCR0.B.WOMQ = 0;                        // 0 = Pins designated for output by DDRQS operate in normal mode.
    QSMCM.SPCR0.B.BITS = 0b1000;                // 8 bits per transfer
    QSMCM.SPCR0.B.CPOL = 0;                        // Clock polarity.
    QSMCM.SPCR0.B.CPHA = 1;                        // Clock phase.
    QSMCM.SPCR0.B.SPBR = 0x03;                    // 6.66mhz value between 2-255  fsys/(2*0x03) = 6.66E6
   
   
    QSMCM.SPCR1.B.DSCKL = 0x2;                    // 50 nano second delay (PCS to SCK Delay) 1 to 127
    QSMCM.SPCR1.B.DTL = 0xFF;                    // Length of delay after transfer. 1 to 255
   
   
    QSMCM.SPCR2.B.WREN = 0;                        // disable wrap around mode
    QSMCM.SPCR2.B.WRTO = 0;                        // Wrap to pointer address 0x0
                                                // these settings disable spi after completion

    QSMCM.SPCR2.B.ENDQP    = 0x0;                    // Ending queue pointer. [application should only move endqp]
    QSMCM.SPCR2.B.NEWQP    = 0x0;                    // New queue pointer value.


    QSMCM.SPCR3.B.LOOPQ = 0;
    QSMCM.SPCR3.B.HALT = 0;


    // interrupt pins
    QSMCM.SPCR2.B.SPIFIE = 0; // SPI finished interrupt enable.
    QSMCM.SPCR3.B.HMIE = 0;
}





void eeprom_read(unsigned char address, unsigned char *data, unsigned char length)
{
    int i = 0;
   
      QSMCM.SPCR2.B.ENDQP    = 0x1;

       for(i=0; i<=3; i++)
       {
        QSMCM.COMDRAM[i].B.CONT  = 0;
        QSMCM.COMDRAM[i].B.BITSE = 1;
        QSMCM.COMDRAM[i].B.DT    = 1;
        QSMCM.COMDRAM[i].B.DSCK  = 1;
        QSMCM.COMDRAM[i].B.PCS3  = 0;
        QSMCM.COMDRAM[i].B.PCS2  = 0;
        QSMCM.COMDRAM[i].B.PCS1  = 0;
        QSMCM.COMDRAM[i].B.PCS0  = 1;
       }
   
    QSMCM.TRANRAM[0].B = 0x03;        // Send Read OpCode
    QSMCM.TRANRAM[1].B = 0x00;        // high address
    QSMCM.TRANRAM[2].B = 0x10;        // low address   
    QSMCM.TRANRAM[3].B = 0x0;        // dummy data   
   
   
    QSMCM.SPCR1.B.SPE = 1;

    while(QSMCM.SPSR.B.SPIF != 1);


    *data = (unsigned char)QSMCM.RECRAM[3].B;
}


void eeprom_writechar(unsigned int address, char data )
{
    int i = 0;
   
       QSMCM.SPCR2.B.ENDQP    = 0x3;        // Ending queue pointer; 0x0 - 0x1F = 0-31;
                                       // Execution of 0 and 1 commands
    for(i=0; i<=4; i++)
    {
        QSMCM.COMDRAM[i].B.CONT  = 0;     // 0 = Control of chip selects returned to PORTQS after transfer is complete.
        QSMCM.COMDRAM[i].B.BITSE = 1;     // 1 = Number of bits set in BITS field of SPCR0.
        QSMCM.COMDRAM[i].B.DT    = 1;     // 1 = SPCR1 DTL[7:0] specifies delay after transfer PCS valid to SCK.
        QSMCM.COMDRAM[i].B.DSCK  = 1;     // 1 = SPCR1 DSCKL[6:0] specifies delay from PCS valid to SCK.
        QSMCM.COMDRAM[i].B.PCS3  = 0;
        QSMCM.COMDRAM[i].B.PCS2  = 0;
        QSMCM.COMDRAM[i].B.PCS1  = 0;
        QSMCM.COMDRAM[i].B.PCS0  = 1;    // select this spi device for serial receive & transfer
            // up to 32 commands;
    }

   
    QSMCM.TRANRAM[0].B = 0x06;                // Write Enable prior to Write   
    QSMCM.TRANRAM[1].B = 0x02;                // Send Write OpCode
    QSMCM.TRANRAM[2].B = 0x00;                // high address
    QSMCM.TRANRAM[3].B = 0x11;                // low address   
    QSMCM.TRANRAM[4].B = data;
        // 16 bits; 32 transmit data blocks
       

    QSMCM.SPCR1.B.SPE = 1;                        // 1 = QSPI is enabled. Pins allocated by PQSPAR are controlled by the QSPI.
                                                // since wrap around is disabled... qspi is disabled after execution of commands

    while(QSMCM.SPSR.B.SPIF != 1);
        // all commands in spi have been completed.
}


0 Kudos
Reply