MPC17531A replacement or alternative part

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC17531A replacement or alternative part

Jump to solution
488 Views
mithunp_s
Contributor III

Dear All,

One of my customer wants to drive a bipolar step motor and maximun output current of 0.7A.

Customer has chosen MPC17531A but we found this series is not recommended for new designs and there is no replacement part also available.

Please advise if suitable part is available in freescale which can meet customer requirement.

Thanks in Advance

Regards

Mithun

0 Kudos
1 Solution
407 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mithun,

Then I would recommend considering the MC34933, it is also a dual H-bridge with an ambient operating temperature up to 85°C.

Regards,

Tomas

View solution in original post

0 Kudos
3 Replies
407 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Mithun,

Most of our dual, low power H-bridges are mature. However, both the MPC17529 and MPC17533 are still active parts and meet customer’s requirements.


Regards,

Tomas

0 Kudos
407 Views
mithunp_s
Contributor III

Hi Tomas,

Thanks for your inputs, sorry I missed out to mention the temperature range customer need a part supporting up to -20 to 80deg, the parts mentioned above from you support upto 60deg.

Your suggestions are really valuable.

Thanks & Regards

Mithun

0 Kudos
408 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mithun,

Then I would recommend considering the MC34933, it is also a dual H-bridge with an ambient operating temperature up to 85°C.

Regards,

Tomas

0 Kudos