MMZ25332B PA from 3.6V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMZ25332B PA from 3.6V

1,034 Views
edwin_spector
Contributor I

Similar to an earlier question, (on MMZ09332BT1) how to calculate bias resistors for 3.6V operation? The datasheet gives some values for 3.3V, but 500 & 90 Ohms are non-standard, so I wondered how critical they were. 

I may try interpolating between the values for 3.3V and 5V, but it would be helpful to know what bias currents to set.

Ref: https://www.nxp.com/docs/en/data-sheet/MMZ25332B.pdf?pspll=1 

Thanks

Edwin.

Tags (1)
0 Kudos
4 Replies

798 Views
LPP
NXP Employee
NXP Employee

Unfortunately I do not have a guide on-hand for adjustment of bias resistors with Vdd=3.3 or 3.6V.  I did however, a guide for adjusting bias resistors with Vdd=5.0V.  I hope that is helpful. Please, I sent it to you directly.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

798 Views
sumitk
Contributor I

Hi LPP, can you also send to me? Thanks

0 Kudos

798 Views
drid
Contributor I

Also interested, can you send it to me too?

0 Kudos

798 Views
drid
Contributor I

I am also interested in that, can you send it to me too?

Thanks

0 Kudos