MM5Z15V Related

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM5Z15V Related

414 Views
erintse01
Contributor I

hello everyone,

 

The question is What is the maximum power dissipation that can be safely handled by the MM5Z15V  Zener diode when it is used as a voltage regulator in a circuit that has a maximum output current of 20mA?

#MM5Z15V
Tags (1)
0 Kudos
Reply
2 Replies

102 Views
Dyethin01
Contributor I

MM5Z15V is commonly used for voltage regulation and protection, and the "15" in the part indicates that the diode Zener voltage is 15 volts.

0 Kudos
Reply

394 Views
pavla_hajna
NXP TechSupport
NXP TechSupport

hello Erin Tse,

MM5Z15V is Nexperia product: https://www.nexperia.com/search.html?searchCategory=&q=MM5Z15V

Please contact Nexperia for further support: https://www.nexperia.com/support/

Have a nice day

Pavla

0 Kudos
Reply