Hi,
I've noticed that when I start a debug session, and it gets to main() and pauses as normal, if I don't start the run within a certain time frame, it seems to crash and I get this call stack:
McuEmbedWhiteChip JLink Release [GDB SEGGER Interface Debugging]
McuEmbedWhiteChip.axf
Thread #1 57005 (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
0xdeadbeee
arm-none-eabi-gdb (12.1.90.20221210)
I haven't timed this, but it seems to be within a minute or two.
Any ideas please?
Info:
Kind regards.
Hello,
Thank you for contacting NXP support.
I appreciate the information, but before continuing the support can you please help me by updating the MCUXpresso version 11.9.0. Also if it is possible can you please help me y telling me if you are running an specific SDK or if this event happens on general.
In case this is a custom project please help me by testing with a hello_word example just to have another point to start.