MC33772, CT pins max voltage?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33772, CT pins max voltage?

Jump to solution
366 Views
CarlosOrendain
Contributor I

What is the absolute maximum voltage rating on CT pins?

CarlosOrendain_0-1665603052561.png

Datasheet only have the differential voltage range and this note:

CarlosOrendain_2-1665603133434.png

 

I want to know if the MC33772 is able to survive a short to battery (12V) in any of the CT pins.

0 Kudos
Reply
1 Solution
317 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please note that 6.7V is valid under permanent operation, and even in such case some margin has been taken (the value might have been higher). 

View solution in original post

0 Kudos
Reply
1 Reply
318 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please note that 6.7V is valid under permanent operation, and even in such case some margin has been taken (the value might have been higher). 

0 Kudos
Reply