Can anyone tell me what current the device should draw after the radio has been initialized (e.g. ResetMaca();
MLMERadioInit() but not yet transmitting or receiving?
I am getting around 3.9 ma before initializing the Radio and 8.54 after. On transmit I get 32.2 mA.
It seems to me from my understanding of the documentation that initializing the radio should not significantly increase the current. Also, the amount that it increases looks to be added to the transmit current (should be 29 mA).
Thanks,
Brillo
Brillo wrote:Can anyone tell me what current the device should draw after the radio has been initialized (e.g. ResetMaca();
MLMERadioInit() but not yet transmitting or receiving?
I am getting around 3.9 ma before initializing the Radio and 8.54 after. On transmit I get 32.2 mA.
It seems to me from my understanding of the documentation that initializing the radio should not significantly increase the current. Also, the amount that it increases looks to be added to the transmit current (should be 29 mA).
Thanks,
Brillo
Here are my results:
http://devl.org/pipermail/mc1322x/2009-May/000003.html
MLMERadioInit is probably leaving the radio on. I wrote radio_off and radio_on routines to turn the radio off and on again without re-initializing. You can find them here:
http://git.devl.org/?p=malvira/libmc1322x.git;a=blob;f=lib/maca.c
-Mar.
Mar,
Thank you. I had already found these and in fact used the radio_of function. Turning the radio off after MLMERadioInit does reduce the current by around 4 mA.
So, has it been your experience that with the radio on but not transmitting or Receiving packets that you get an additional 4 ma of current?
Again, my continuous transmit (nomod) current is also up by about 4 mA from the published 29 mA.
If so, your functions are going to be very helpful.
Thank you much,
Brillo
Mar,
Sorry. In haste I failed to read your test results.
Thanks you again!
Brillo