Looking for NXP Evalution board with espi support with master.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for NXP Evalution board with espi support with master.

550件の閲覧回数
gauravsuryavans
Contributor II

Hi Community,

I am looking for evalution board with have pin out for espi as master, is there any board from NXP.

Any help would be appreciated.

Regards,

Pankaj

タグ(1)
2 返答(返信)

458件の閲覧回数
Pavel
NXP Employee
NXP Employee

For example see the following boards:

P5040RDB, P1022DS, P1023RDB, P1024RDB, P1025RDB, TWR-P1025

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

458件の閲覧回数
gauravsuryavans
Contributor II

Hi PavelChubakov‌,

Thanks for answering.

Regards,

Pankaj

0 件の賞賛