I'd like to use the ATF05MS003N in the 72-76 MHz band.
The datasheet reference circuit gives Zsource and Zload values for frequencies from 135-174 and 350-520 MHz.
The S parameter file covers 240-1000 MHz.
A similar question mentioned the AFT05MS003N_PDK file, which no longer exists.
How can I get the input and output impedance values for my frequency range (72-76 MHz)?
AFT05MS003N is conditionally stable and may require stability enhancement. For your frequency band, applying series 12 Ohm + shunt 27 Ohm resistors at the gate makes amplifier unconditionally stable.
I performed load pull simulation using ADS model of this transistor.
Vdd=7.5V, Idq=80mA
Zload = 12.54 + j6.24
Zinput = 14.32 - j9.1
Input impedance as measured from input series resistor to ground.
Amplifier schematics and performance at 74MHz are attached.
Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------