LX2160 YOCTO build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160 YOCTO build error

78 Views
ranga_yn
Contributor III

Hello team,

I am on Ubuntu :

Distributor ID: Ubuntu
Description: Ubuntu 20.04.4 LTS
Release: 20.04
Codename: focal

Below is the error on my build , If any patch to replace on the board do let me know , I followed are the pre requisite for the build once.

ERROR: Logfile of failure stored in: /YOCTO_BSP/build_lx2160ardb-rev2/tmp/work/x86_64-linux/binutils-cross-aarch64/2.38-r0/temp/log.do_unpack.261346
ERROR: Task (/YOCTO_BSP/sources/meta-nxp-desktop/recipes-devtools/binutils/binutils-cross_2.38.bb:do_unpack) failed with exit code '1'

 

Thanks,

Ranga

 

0 Kudos
1 Reply

69 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Could be some fails in fetching arise to this error or bad image download, please try to erase everything from yocto and restart again if the same fails is present you have to download the correct image.

 

Regards

 

0 Kudos