LTIB first run does not complete on OpenSuse 12.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB first run does not complete on OpenSuse 12.1

Jump to solution
569 Views
ChrisLaRocque
Contributor II

Hello

 

I have one system which works; Open Suse 11.4

And one which doesn't; OpenSuse 12.1

 

the same error is reported both with a cvs download from Savannah and the CD that came with my 8308RDB

 

Differences

 

Ver 11.4, found all required packages for ltib

Ver 12.1, had to install rpm-build from the OpenSuse "Factory" repository.

 

The fault reported

 

"

ln: failed to create symbolic link `/tmp/rpm-clarocque/BUILDROOT/rpm-fs-4.0.4-1.x86_64/opt/ltib/usr/lib64/rpm/rpmt': No such file or directory

"

 

The directory rpm exists but there is nothing in it.

 

There are errors about librpm components not being present in lib64 but they seem to have been built without error.

 

There are some messages found on google with a similar reported failure but no definitive answers.

 

Attached is the host_config.log

 

Can someone give me some direction please?

 

Regards

 

Chris LaRocque

 

0 Kudos
1 Solution
375 Views
ChrisLaRocque
Contributor II

I installed OpenSuse 11.4 on this machine and ltib worked just fine. Don't have time to determine why this happened.

 

C

View solution in original post

0 Kudos
1 Reply
376 Views
ChrisLaRocque
Contributor II

I installed OpenSuse 11.4 on this machine and ltib worked just fine. Don't have time to determine why this happened.

 

C

0 Kudos