LDMOS PA in class D or E possible ???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LDMOS PA in class D or E possible ???

704件の閲覧回数
johnjackson
Contributor I

Forum, I am looking into designing a class D or E high efficiency amplifier operating at 80MHz for a laser ignition system.  I have designed a lot of amplifiers with LDMOS but all were class AB.  I don't see anything online about using LDMOS in these switch mode architectures.  Am I missing something or is there some issue or problem with using LDMOS in these conditions.

Thanks,

John Jackson

rfrus1@gmail.com

ラベル(1)
  • RF

0 件の賞賛
返信
1 返信

492件の閲覧回数
milanbaca
Contributor III

Yes it is possible to use LDMOS PA in class D or E.

0 件の賞賛
返信