Kernel Ver 2.6 not booting IN MPC8555CDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel Ver 2.6 not booting IN MPC8555CDS

1,858 Views
sabarinath
Contributor I
    hai friends,
i am using powerPC  Product name: “SPTWIMAXCC1E” AMC Channel Card ,and i used LTIB to build the kernel ver2.6 i used theLTIB version  MPC8555CDS_20061017-ltib.iso , i installed LTIB configured  the kernel and tried to boot in “SPTWIMAXCC1E” AMC Channel Card unfortunalely the error showing can you tell what is the problem happend here "ADVANCE THANKS"

=> bootm 1000000

## Booting image at 01000000...

   Image Name:   Linux-2.6.11

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

   Data Size:    1332056 Bytes = 1.3 MB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

mpc85xx_cds_init(): exitImage ... OK

id mach(): done

MMU:enter

MMU:hw init

MMU:mapin

MMU:setio

MMU:exit

setup_arch: enter

setup_arch: bootmem

HERE IT STUCKED........................

PLEASE HELP


Tags (1)
0 Kudos
Reply
1 Reply

670 Views
gunda
Contributor I
hey sabarinath dont worry it will boot up

RK will make all changes and u can tell every one that u booted up and  u can get in as a employee here

hahaha!!....hahah....hahah!!!

???:smileyhappy::smileyvery-happy::smileywink::robotmad::womanhappy::womansad::smileysad::smileysurprised::manmad:
0 Kudos
Reply