Hello
I'm using the JN-5189 DK with the example JN-AN-1246, everything is working good but I'm facing a problem that when my device wakes up from sleep it took 60ms to wake up and consume 3 to 4 mA current.
Attached is the photo of the oscilloscope showing the sensor time taken after wakeup and current consumption.
I'm at the end of the project and I need to minimize the size of the pulse so it can drain the minimum current.
kindly help me out.
Thank You
Regards Talha