Iperf TCP Throughput Testing of SJA1105SMBEVM as simple switch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Iperf TCP Throughput Testing of SJA1105SMBEVM as simple switch

4,215 Views
ivan_kenetics
Contributor II

Can RDDRONE-T1ADAPT be used as a Media Converter for Iperf TCP Throughput test for testing the SJA1105 Performance as a simple switch based on the attached block diagram?

 

Labels (1)
0 Kudos
Reply
9 Replies

3,461 Views
iaingalloway
NXP Employee
NXP Employee

Just noticed this thread, but our testing of RDDRONE-T1ADAPT between a laptop and an I.mx 8Mplus board using iperf gave 95-98mbps.

0 Kudos
Reply

4,204 Views
andrei_skok
NXP Employee
NXP Employee

I don't see any problem to use the RDDRONE-T1ADAPT as a Media Converter based on the attached block diagram. 

0 Kudos
Reply

4,064 Views
kylefu
Contributor I

@andrei_skok 

Hello, I use the  RDDRONE-T1ADAPT  to test, but it looks like sometimes the network will down briefly.

Is there a new firmware for RDDRONE-T1ADAPT?

Could you help me to fix it?


来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
请求超时。
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=1ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=1ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
请求超时。
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
请求超时。
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
请求超时。
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
请求超时。
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128
来自 192.168.1.155 的回复: 字节=32 时间=2ms TTL=128

 

0 Kudos
Reply

4,054 Views
ivan_kenetics
Contributor II

I didn't get the  RDDadRONE-T1ADAPT to test as there is no ready stock at the point when I asked the question but looking at your problem, I would suggest you look at the 100Base-T1 Link LED first. If the LED goes off sometime during your test, you'll probably need to look at your physical connection between the test boards, and also what type of cable and length of cable you're using.

 

0 Kudos
Reply

4,045 Views
kylefu
Contributor I

If possible, could you please help to send me a latest firmware or software to me, thank you so much.

0 Kudos
Reply

4,035 Views
ivan_kenetics
Contributor II

I'm not using RDDadRONE-T1ADAPT  for testing and thus I don't have the firmware / software for it. You may need to contact the FAE or tech support to get it. Also your ping test response time of 2ms indicate something is not right. Normally the response time should be <1ms with a cable length of up to 15 meters for a good stable T1 connection unless you're going through a number of ethernet switches between your computer and the ethernet port of the converter.

0 Kudos
Reply

3,990 Views
kylefu
Contributor I

@ivan_kenetics 

Thank you so much!

Yes, I use the RDDadRONE-T1ADAPT to communicate with a converter. So, that is reasonable :).

Thanks for your huge help. I will reach out local FAE.

0 Kudos
Reply

4,048 Views
kylefu
Contributor I

>>I would suggest you look at the 100Base-T1 Link LED first. If the LED goes off sometime during your test,

@ivan_kenetics  Thank you for your reply. I am sure the T1 link LED is always ON, the network is temporarily off. that is why I confused.

I think the cable is not care any more, T1 should have good robustness...

0 Kudos
Reply

4,203 Views
ivan_kenetics
Contributor II

Is there any available iperf throughput result for the RDDRONE-T1ADAPT? The distributor's FAE mentioned to me that NXP recommend to use TECHNICA 100BASE-T1 NXP (Part Number: TE-1600) 100BASE-T1 MediaConverter NXP - Technica Engineering (technica-engineering.de) when I query about using RDDRONE-T1ADAPT. The reason being that they've been using Technica Media converter for their testing (iperf TCP throughput with SJA1105 is around 95Mbits/sec) and that RDDRONE-T1ADAPT is for drone application. 

I'm getting the media converter to do some testing on the SJA1105 as I'm only getting about 60Mbits/sec from Laptop to S32K148EVB with TJA1101 Adapter Card (as Iperf2 Server) and about 30Mbits/Sec from S32K148 (server) to laptop (client) using iperf2 "-r" option.

I need to set the baseline for the SJA1105EVM first before I do further testing and bring it into the target application environment that we intend to use 100Base-T1 network.

So can I assume that the performance of the RDDRONE-T1ADAPT will be on par with TECHNICA 100BASE-T1 NXP media converter?

0 Kudos
Reply