In which USB Type-C port state the CON_DET pin of PTN5150 is asserted?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In which USB Type-C port state the CON_DET pin of PTN5150 is asserted?

444 Views
yhara
Contributor II

We would like to use PTN5150 to realize a DRP / DRD port with only USB 2.0 data lanes without USB-PD support.

In which state (as defined by USB Type-C standard) does PTN5150 asserts CON_DET pin? The datasheet only says it is asserted when a connection is detected, which is not very clear.

Background: an MCU in our system has an input pin that expects high when VBUS is valid and low when invalid. VBUS being valid corresponds to Attached.SRC and Attached.SNK states as defined by USB Type-C standard. We would be able to use CON_DET to drive this pin of the MCU, if CON_DET gets asserted only in Attached.SRC and Attached.SNK states, which is what I am curisous to know.

Tags (4)
0 Kudos
Reply
3 Replies

327 Views
yhara
Contributor II

So, USB Type-C standard defines numerous port states. A port may be in one of several states when a cable or another port is connected to it.

What I would like to know is, in which of those states does PTN5150 assert CON_DET signal.

Please do let me know if my question does not make sense.

0 Kudos
Reply

418 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hello:

This pin will automatically switch from input to CON_DET output in
"non-I2C mode or set 09H bit[0] to 0" after TINPUTLATCH
• CON_DET = High (Connection Detected)
• CON_DET = Low (No Connection)

So I think asserted means 'High' in CON_DET.

0 Kudos
Reply

414 Views
yhara
Contributor II

Thanks. I know it is an active-high signal.

What I want to know is the conditions in which it is asserted. In other words, when does the device detect connection? Or what is the definition of "connection" here?

0 Kudos
Reply