Ideal NFC antenna inductance for PN7642

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ideal NFC antenna inductance for PN7642

Jump to solution
452 Views
KLL
Contributor II

Is there an ideal inductance for NFC antennas working with the PN7642?  The PN7160 antenna design guide states "Out of experience it turns out to be optimum to have an inductance around L ≈ 1 µH for
a proper matching. But a wide range of L ≈ 300 nH up to L≈ 3 µH can be still matched
properly."  Does this apply to other NFC ICs as well, such as the PN7642?

0 Kudos
Reply
1 Solution
368 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @KLL 

Yes, you are right

Please refer to AN11706:  PN7462 family Antenna design guide, page 13

Out of experience it turns out to be optimum to have an inductance around L ≈ 1μH for a proper matching, but a wide range of L ≈ 300nH up to L≈ 4μH still can be matched properly, so typically 1 up to 4 turns in the normal range of antenna sizes are used.

 

Regards

Daniel

View solution in original post

1 Reply
369 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @KLL 

Yes, you are right

Please refer to AN11706:  PN7462 family Antenna design guide, page 13

Out of experience it turns out to be optimum to have an inductance around L ≈ 1μH for a proper matching, but a wide range of L ≈ 300nH up to L≈ 4μH still can be matched properly, so typically 1 up to 4 turns in the normal range of antenna sizes are used.

 

Regards

Daniel