Hello team,
currently when i build the image and flash its vfat for boot and rootfs is ext4 - can the image be supported with XFS , if yes how to do the same any steps.
imx-image-core-imx93evk.rootfs-20240504074502.wic.zst
If the above is not possible and want to have extra partition - of xfs will that be supported if yes , can some one guide the same
Thanks
R
Hello,
Yes Yocto BSP support server-side copy for CIFS, NFS, XFS, support for hard discs with host-managed SMR (Shingled Magnetic Recording).
Regards