I2C for P71D600

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C for P71D600

139件の閲覧回数
czhao
Contributor I

Dear sir:

I use Aduino to control P71D600 and I2C. It seems that I can successfully get the ATR. However, when I use any APDU command under IBLOCK, I never get the correct APDU response code.
21:40:23.116 -> ATR Response:
21:40:23.151 -> Response data:
21:40:23.151 -> A5 EF 25 1 A0 0 0 3 96 4 3 E8 0 FE 2 B 3 E8 0 1 0 0 0 0 64 13 88 C 0 67 50 37
21:40:23.151 -> End of response.
21:40:23.151 -> Sending I-Block with SELECT AID APDU:
21:40:23.184 -> 5A 00 05 00 A4 04 00 00
21:40:23.184 -> CRC Sent: 1E 3C
21:40:23.184 -> I2C transmission successful.
21:40:23.184 -> Awaiting response:
21:40:23.184 -> Response data:
21:40:23.216 -> A5 82 0 DA 4F FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF
21:40:23.216 -> End of response.

Don't know what went wrong

0 件の賞賛
1 返信

116件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @czhao ,

 

Actually P71D600 is not a mass market product which is allowed to discuss it here. Please kindly request NDA at first and request the user manual from the secure file. Please kindly refer to the following for details.

Kan_Li_0-1714029491513.png

 

https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf

Any further issue with doc request, please kindly contact the doc store team via support.docstore@nxp.com 

 

Any further technical issue on this part, please kindly create a private ticket.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛