How to set the SJA1110-EVM device ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set the SJA1110-EVM device ID

749 Views
eric_yf
Contributor I

I'm trying to read the device ID from the SJA1110-EVM which my company bought from NXP recently. Please check the attachment. The device ID of two chips that I read both are 0xFFFFFFFF. But the document descriptions are 0xB700030F, I've been checked other Docs. But I didn't found the way to set the device ID and I could not use python script(setup_sja1110evm.py) to setup up the box. I will be appreciated that someone could help to solve this question! BR.  

Tags (1)
0 Kudos
1 Reply

732 Views
andrei_skok
NXP Employee
NXP Employee

Hello,

Do you have any progress on this?

0 Kudos