HI All,
trying to flash openwrt firmware on LS-1088a but stuck on tinydistro with no ethernet connection
if any Uboot steps will be helpful or do i have to flash uboot, kernel image and rootfs sepratly?
hi @yipingwang
both mac address is set on uboot.
i am trying to flash LS1088ARDB openwrt firmware on LS1088ARDB-PB and after changing ddr_init.c file i am stuck on below error
"BL2: Booting BL31"
eth10addr=68:05:ca:2e:50:ab
eth11addr=68:05:ca:35:c3:1a
eth1addr=00:04:9f:06:eb:71
eth2addr=00:04:9f:06:eb:72
eth3addr=00:04:9f:06:eb:73
eth4addr=00:04:9f:06:eb:74
eth5addr=00:04:9f:06:eb:75
eth6addr=00:04:9f:06:eb:76
eth7addr=00:04:9f:06:eb:77
eth8addr=00:04:9f:06:eb:78
eth9addr=00:04:9f:06:eb:79
ethact=DPMAC1@xgmii
ethaddr=00:04:9f:06:eb:70
Why did you modify ddr_init.c in ATF source code?
It seems that there is DDR controller initialization problem on your target board.
hi @yipingwang
due to ERROR: mmap_add_region_check() failed. error -22 this error i changed ddr_init.c
as solution provided in below link
Hi
static const struct board_timing udimm[] = {
{0x04, rce, 0x01030508, 0x090b0d06},
};
-------------
After change:
-------------
static const struct board_timing udimm[] = {
{0x04, rce, 0x01030508, 0x090b0d06},
{0x0F, rce, 0x01030508, 0x090b0d06},
};
can we flash LS1088ARDB openwrt firmware on LS1088ARDB-PB?
Please refer to target/linux/layerscape/README provided in OpenWRT to build and deploy the image to the target board.
* u-boot may fail to read MAC addresses from EEPROM on some boards and there
won't be MAC addresses set in environment. This may cause kernel fails to
probe these network interfaces. The workaround is to set MAC addresses
manually, for example,
=> setenv ethaddr 00:04:9F:04:65:4b
=> setenv eth1addr 00:04:9F:04:65:4c