How to download LPC54016 FW by keil tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download LPC54016 FW by keil tool

5,665 Views
afzhang
Contributor I

Our project used  LPC54016JET100  chip.I download demo project program by keil tool,but can not download.The keil tool appears an error.That error is "Error :Flash Download failed".How to download program by keil tool correctly!

0 Kudos
Reply
8 Replies

5,493 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 爱飞 张,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Before answering the question, I'd like to know which board and demo project you used for testing.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,493 Views
afzhang
Contributor I

Dear jeremyzhou:

The board is ours.The type of chip is LPC54016JET100.I used “hello_world “demo and “usart” demo.

B/R

Aifei Zhang

发件人: jeremyzhou

发送时间: 2019年11月21日 10:12

收件人: Aifei Zhang

主题: You have been mentioned by jeremyzhou in Re: How to download LPC54016 FW by keil tool in NXP Community

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

You have been mentioned

by jeremyzhou <https://community.nxp.com/people/jeremyzhou?et=notification.mention> in Re: How to download LPC54016 FW by keil tool in NXP Community - View jeremyzhou's reference to you <https://community.nxp.com/message/1235430?commentID=1235430&et=notification.mention#comment-1235430>

0 Kudos
Reply

5,493 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 爱飞 张,

Thanks for your reply.
According to the below figure, the Keil supports to program these three QSPI flash. So I guess the root cause of the programming failure is that the QSPI chip on your board is not listed in Figure 1.

pastedImage_1.png

                                                                     Fig 1

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,493 Views
afzhang
Contributor I

Hi jeremy:

hi Jeremy, The picture above shows the connection method and flash model of our company's flash .I have two questions. Apart from keil tool, do other tools support other flash downloads? Whether three QSPI flash is necessary if the program can be downloaded?

B/R

Aifei Zhang

发件人: jeremyzhou

发送时间: 2019年11月21日 15:19

收件人: Aifei Zhang

主题: Re: - Re: How to download LPC54016 FW by keil tool

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: How to download LPC54016 FW by keil tool

reply from jeremyzhou <https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> in Other NXP Products - View the full discussion <https://community.nxp.com/message/1235650?commentID=1235650&et=watches.email.thread#comment-1235650>

0 Kudos
Reply

5,493 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 爱飞 张,

Thanks for your reply.
1) Do other tools support other flash downloads?
-- I'd like to suggest you use the MCUXpreeso IDE.
1) Whether three QSPI flash is necessary if the program can be downloaded?
-- For MCUXpresso, it can support to program other QSPI in addition to these three QSPI flash.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,493 Views
afzhang
Contributor I

Hi Jeremy:

I try the MCUXpreeso IDE. I try to import the project, but the situation above appears. How can I solve the problem!

B/R

Aifei Zhang

发件人: jeremyzhou

发送时间: 2019年11月22日 14:57

收件人: Aifei Zhang

主题: Re: - Re: How to download LPC54016 FW by keil tool

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: How to download LPC54016 FW by keil tool

reply from jeremyzhou <https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> in Other NXP Products - View the full discussion <https://community.nxp.com/message/1236173?commentID=1236173&et=watches.email.thread#comment-1236173>

0 Kudos
Reply

5,493 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 爱飞 张,

Thanks for your reply.

According to the above figure, the MCUXpresso hasn't installed the SDK for LPC5401x, so I've attached MCUXpresso_IDE_User_Guide, it presents how to install the SDK library in Chapter 6, please refer to it for details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,493 Views
afzhang
Contributor I

Hi Jeremy:

Thanks!

B/R

Aifei Zhang

发件人: jeremyzhou

发送时间: 2019年11月25日 11:05

收件人: Aifei Zhang

主题: Re: - Re: How to download LPC54016 FW by keil tool

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: How to download LPC54016 FW by keil tool

reply from jeremyzhou <https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> in Other NXP Products - View the full discussion <https://community.nxp.com/message/1236756?commentID=1236756&et=watches.email.thread#comment-1236756>

0 Kudos
Reply