How to construct Ethernet over PCIe for S32V234

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to construct Ethernet over PCIe for S32V234

Jump to solution
388 Views
soccercheng
Contributor I

I have the following questions about constructing the development environment using the Ethernet over PCIe on S32V234

  • Which PICe switch with NTB support should I use ?
  • Do I need a PC as root complex ?
  • Any software packages that are required ? and how do I get the source code ? 

 

BTW,

Is there a tutorial for this ?

0 Kudos
1 Solution
377 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

For general recommendation about PCI There the hardware desing guide of S32V234 EVB:

https://usermanual.wiki/m/90e50b774edd0ff1c5f73f64c4f8f10644afa6d9a8e77532e18c344c1e681e38.pdf

 

For PCI enumeration please follow the user guide of the linux BSP:

 

Regards

View solution in original post

0 Kudos
2 Replies
378 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

For general recommendation about PCI There the hardware desing guide of S32V234 EVB:

https://usermanual.wiki/m/90e50b774edd0ff1c5f73f64c4f8f10644afa6d9a8e77532e18c344c1e681e38.pdf

 

For PCI enumeration please follow the user guide of the linux BSP:

 

Regards

0 Kudos
353 Views
soccercheng
Contributor I

Hello,

Many thanks for your input, I've found the information I need in the user manual and Linux BSP.

But I've got little confused about the following architectural questions

  • Why, in BSP 23.5, the "vnet"  driver is only included in s32v234bbmini, but not in s32v234evb and s32v234pcie ?
  • In the PCIe Virtual Ethernet sample application, S32V234-EVB running as RC and the S32V234-PCIE running as EP.
    • Does this mean EVB and PCIE can talk to each other through socket connection only ? Is the EVB able to play as an NAT and route the socket packet to EXTRANET ?

THANX 

0 Kudos