Hello, as title, I tried to let OV/OT fault occur, the FAULT1_STATUS could detected the fault, however, the FAULT pin remain in low level. even I tried to let FAULT_DIAG set to 1, FAULT pin still stay in low level.
What kind of condition or situation, when FALUT occur then trigger the FAULT pin to High level.
Thanks for any help.
Mark
For the OV please refer to:
When unmasked by FAULT_MASK1[MASK_12_F], the FAULT1_STATUS[VPWR_OV_FLT] bit sets the FAULT output pin high. An overvoltage condition on the VPWR pin does not cause the 33771 to perform a shutdown. The pack controller may clear the FAULT1_STATUS[VPWR_OV_FLT] bit when VPWR returns to the normal operating range by writing logic 0 to the FAULT1_STATUS[VPWR_OV_FLT] bit.
Thanks for your reply.
Right now I can let the FAULT pin activate, one more question related wake-up event.
I just want to MASK UV event,
1. I tried to set FAULT_MASK1[MASK_0F] = 0x1
2. WAKEUP_MASK1[MASK_0F] = 0x1
3. goto sleep, then [the let UV event happened,
4. the FAULT pin activate and system wake-up
if FAULT_MASK1 = 0xf and WAKEUP_MASK1 =0xf, UV event happened, system won't wake-up.
it means I MUST setting UV/OV/UT/OT event at the sometime(value = 0xF), cannot setting individual event only one of (UV/OV/UT/OT).