How to change the Vref of ltc2442 from 2.5 to 5V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the Vref of ltc2442 from 2.5 to 5V

418件の閲覧回数
alphy
Contributor I

I am interfacing LTC2442 24-bit ADC with my TM4C123(Tivaware)microcontroller. I am able to read up to 2.5V analog input voltage. If I am giving more than 2.5V then there is no change in output voltage, It is giving 2.5V only. So my doubt is how I can set the Vref to 5V, Is there any commands for setting the vrefernce. I am operating the device in Single Mode.

In my project I need to read more than 2.5V. So please let me know what I can do for this.

Thank you,

Alphy

0 件の賞賛
返信
0 返答(返信)