How about the state of DP&DN pins of PTN3222CUK when in reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How about the state of DP&DN pins of PTN3222CUK when in reset

Jump to solution
451 Views
huynhdangminh
Contributor I

How about the state of DP&DN pins of PTN3222CUK when the reset signal RST_N is asserted? (Hi-Z? Pull-Down? Pull-Up? No-change?)

And if it is not the Hi-Z state, is there any way to change the state of DP&DN to Hi-Z when in reset?
(For example, cut down the 3.3 V power line when in reset or something like that)

0 Kudos
Reply
1 Solution
436 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

When reset pin of PTN3222CUK is asserted, USB2 interface is Hi-Z with 2M ohm pull down on D+/D-.

View solution in original post

0 Kudos
Reply
2 Replies
437 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

When reset pin of PTN3222CUK is asserted, USB2 interface is Hi-Z with 2M ohm pull down on D+/D-.

0 Kudos
Reply
432 Views
huynhdangminh
Contributor I

I got this. Thank you for your support.

0 Kudos
Reply