Help for MHVIC915NR2 design files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help for MHVIC915NR2 design files

819 Views
jammal
Contributor I

any one can help me get s2p file and model for 

MHVIC915NR2 transistor 

Labels (1)
  • RF

Tags (1)
0 Kudos
Reply
2 Replies

811 Views
andrei_skok
NXP Employee
NXP Employee
All PFP16 PACKAGED DEVICES including MHVIC915NR2 were discontinued in 2012.
 
The MHVIC915NR2 was replaced by the MW7IC915NT1.
 
We don't have any design files for the MHVIC915NR2. 
 
All design files for the MW7IC915N can be found on the Product page
 
0 Kudos
Reply

809 Views
jammal
Contributor I

I know it is old part , but I have some of it and I need to make design for it 

nxp must have the file in database , it is not good that make transistor and sell it then after 10 year there is no file for it ! 

what I should do with the transistor that I have now ? 

Tags (1)
0 Kudos
Reply